1/21/2013 3:49 PM | |
Joined: 9/23/2005 Last visit: 3/14/2025 Posts: 4406 Rating:
|
Hi, The S7-1200 CPU haven't PROFIBUS ports but you can use CM to do it (as master or as slave) There is no High Speed counter that should be uses as expansion module for S7-1200 (in central rack) Sorry, I mean IM151-8, ET200S CPU You can get examples of communication in the forum at https://www.automation.siemens.com/BR/tf/WW/en/Posts/68281 You can just useuse technological objects (Axis) and instructions (MC_MoveAbsolute, etc,...) with internal inputs / outputs of the CPU (or SB) |
Denilson Pegaia |
|
Follow us on