1/31/2024 9:42 AM | |
Joined: 8/3/2017 Last visit: 6/11/2024 Posts: 1086 Rating: (53) |
Hello mohitkataria012, please be patient, as no one is obliged to reply in the forum (see forum terms). If you want an official answer, please submit a Support Request. Regarding your question: Can you tell us in more detail what you have tried so far and where you got stuck (maybe you can attach a screenshot, as a picture tells more as words)? Which SCADA are you talking about? Which SEW drive are you using? The same one in your previous topic? 8Noodles |
Please, check out the forum search to find already existing topics regarding your issue and to get some hints. |
|
2/1/2024 4:16 PM | |
Joined: 6/24/2013 Last visit: 9/13/2024 Posts: 1623 Rating: (421)
|
Hi for SEW Movidrive servo with Profibus: You need configure drive itself to use signals via Profobus (and scaling can be done in PLC or in drive) Function which talks to drive attached (as a source which you need to import to your project) remember to add symbol first! and you may need modify function to your application. AttachmentSEW_DRIVE.zip (242 Downloads) |
Follow us on