10/16/2020 9:36 AM | |
Joined: 3/14/2015 Last visit: 10/29/2023 Posts: 93 Rating: (0) |
Dear experts, In a project I need to control a step motor ( 4-phase, 1.8 degree) using a CPU 1200 connected to a Digital Stepping Driver (model: DM556). Can you help me to implement the plc program? should I use motion control technology? Do you have a project to give me? I have attached documents of the driver AttachmentDM556m.pdf (146 Downloads) |
10/21/2020 2:08 PM | |
Joined: 3/30/2020 Last visit: 4/30/2024 Posts: 4469 Rating: (935) |
The very first thing is to consult the following resources..
The last one is the most practical guide. |
Last edited by: qwazee at: 10/21/2020 14:09:08Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
10/21/2020 3:20 PM | |
Joined: 3/14/2015 Last visit: 10/29/2023 Posts: 93 Rating: (0) |
you mean that the same thing goes for controlling a step motor with a DM556 drive ? |
10/21/2020 4:48 PM | |
Joined: 3/14/2015 Last visit: 10/29/2023 Posts: 93 Rating: (0) |
perfect, I will give it a try |
This contribution was helpful to1 thankful Users |
Follow us on