1/12/2023 1:04 PM | |
Joined: 7/19/2022 Last visit: 8/12/2024 Posts: 380 Rating: (62) |
Hi AutoGen_3097883, It is logical, in simulation if you can activate the inputs by simply clicking with the mouse on ON/OFF. If you want to do it physically you need a button/push button to activate those inputs. You can use the LOGO! Look in the manual: |
If this Information really helps, you could use the Rate function |
|
1/12/2023 1:21 PM | |
Joined: 12/18/2014 Last visit: 8/14/2024 Posts: 33554 Rating: (4168)
|
Your description is a bit difficult to understand. I'm assuming you want to change setpoints. Is it like this? |
Follow us on