Industry Online Support
Technical Forum
3/29/2008 9:55 PM | |
Posts: 15 Rating: (0) |
HOW TO CONVERT AN ANALOGIQUE INPUT FROM KF TO KG AND VIS VERSA IN THE PROGRAM STEP7 OR STEP5 |
3/30/2008 11:09 PM | |
Posts: 15 Rating: (0) |
|
4/4/2008 5:58 PM | |
Joined: 9/23/2005 Last visit: 7/2/2024 Posts: 4347 Rating: (1438) |
Hi, which S5 CPU do you have? |
Denilson Pegaia |
|
4/5/2008 9:16 PM | |
Posts: 15 Rating: (0) |
I think you have understant me , yes I have s5 please show me how to convert from kg to kf and vis versa. THANKS |
4/5/2008 9:19 PM | |
Posts: 15 Rating: (0) |
I HAVE A SIMATIC 135U WITH CPU 928B |
4/9/2008 3:38 PM | |
Posts: 487 Rating: (36) |
The analog input value on a 135U should be from 0 to 2048 ( in KF) this reprsents 0 to 20 mAmp or 0 to 10 volt depending on your input card insert. See if you can download the system manual for 135U (https://support.automation.siemens.com/WW/llisapi.dll/csfetch/1085837/6ES5+998-OSH21.pdf?func=cslib.csFetch&nodeid=1118168&forcedownload=true) Eric |
Follow us on