6/19/2024 5:26 AM | |
Joined: 4/29/2024 Last visit: 6/24/2024 Posts: 3 Rating:
|
Hey, I want to know if I can convert ohms value from PT-100(3-wired) to current or voltage through ladder logic diagram, if yes, then how? ------------------------------------------------------------------------------------------ |
Last edited by: mahima_attri154 at: 06/19/2024 06:10:22Last edited by: The Helping Hand at: 06/19/2024 09:52:36New subject after splitting |
|
6/19/2024 11:36 AM | |
Joined: 5/6/2022 Last visit: 7/5/2024 Posts: 429 Rating:
|
Hi mahima_attri154, In the RTD modules of the S7-1200, where you connect a PT100, you get the value in Cº or Fº. In this section of the manual, the equivalence appears in the last table: I hope it helps |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
6/24/2024 6:07 AM | |
Joined: 4/29/2024 Last visit: 6/24/2024 Posts: 3 Rating:
|
Hey, I have the module 1234 how to use that for the conversion? |
6/24/2024 7:46 AM | |
Joined: 3/30/2020 Last visit: 7/12/2024 Posts: 4624 Rating:
|
You are hoping to use a normal analog card to read the PT-100. This is not recommended for industrial applications. You can consider getting a RTD to analog converter, if you have to. For an academical project you can consider building the converter yourself. Web search "RTD to analog converter" or something like it. For theoretical background, have a look at: https://en.wikipedia.org/wiki/Resistance_thermometer. Especially focus on the one where a 3 wire device is mentioned. |
Last edited by: qwazee at: 06/24/2024 07:47:10Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
Follow us on