5/17/2022 11:23 AM | |
Joined: 4/10/2021 Last visit: 3/21/2024 Posts: 70 Rating:
|
Hi my AS = redundant CPU414-5H + 2 OS (both configured as server) at first I have been developed a program in my laptop as ES, then copied it to both OS, then configured OS , so I had 2 identical OS connected to CPUs. Due to some changes in process description and also installing new equipment in the plant, I changed the program of OS1 and now OS1 is OK and work properly. To update OS2 I opened an archive of OS1 in it and solely copied the plant screens (designed by wincc) from OS1 to proper hierarchy folder of OS2 (NOT copied the CFC nor done any download). at final almost 95% of the screens on OS2 are working OK, but some of them does not work fine (e.g. not showing the actual value or interlocks FP are empty , ...) which I described them in attached pics. (ERRORS.ZIP) Please if anyone have a solution for this problem or any other way to update OS2 and make it similar to OS1 tell me ?? in theory copied screens from OS1 to OS2 should work fine , because they are made based on the codes inside CPU,,,,, but I have some errors..........would you please share any ideas? Thanks Regards Ali Attachmenterrors.zip (218 Downloads) |
Follow us on