Industry Online Support
Technical Forum
1/27/2006 11:32 AM | |
Joined: 8/25/2005 Last visit: 7/5/2024 Posts: 1162 Rating:
|
Hello RUNTIME, if the BF-LED is lightning there are problems depending on the PROFIBUS. Please check wether there is everything ok. Busparameters and so on. Pull of the PROFIBUS cabel and the LED should switch of. A description of the LEDs is given in the following document: S7-CPs Manual/ Part B1 / Part Description of the CP 342-5 / CP 342-5 FO (Teil A siehe Beitrags-ID 1158693) Best regards Sabine |
Follow us on