8/1/2012 12:00 PM | |
Joined: 1/8/2012 Last visit: 8/21/2024 Posts: 17 Rating: (0) |
Hi, I have read this: The CPU 1215C is released for delivery since 10 days. S7-1215C; 3 models: DC/DC/DC; AC/DC/Rly; DC/DC/Rly – 130 mm wide
________________________________________________________________________ so I would like to know, these 2 ports are Ethernet ports right? is it possible to make a network by concatenate the plc's one to another and the last one goes to a PC? or i missunderstood the purpose of the secondery port? thank you. |
8/1/2012 5:32 PM | |
Joined: 9/23/2005 Last visit: 11/4/2024 Posts: 4351 Rating: (1452)
|
Hi, the CPU has two ports. That means that the CPU works like if it would be connected to a Switch with two free ports. So, you can connect two cables at same time. However the CPU has just one IP address. |
Denilson Pegaia |
|
This contribution was helpful to1 thankful Users |
8/12/2012 5:37 PM | |
Joined: 1/8/2012 Last visit: 8/21/2024 Posts: 17 Rating: (0) |
Thank you both for your help. |
Follow us on