10/14/2012 7:50 AM | |
Posts: 1 Rating: (0) |
how i can to configure the cpu 3176TJ100AB0 in a s7 project.?and what additional software do we need? |
10/14/2012 1:07 PM | |||||
Joined: 9/27/2006 Last visit: 6/4/2024 Posts: 12260 Rating: (2670)
|
Hello M.R. Heydarshenas; I believe you need S7-Technology as an add-on package to integrate the Motion Control functions of a T-CPU:
6ES7864-1CC42-0YA5: OPTIONAL PACKAGE S7-TECHNOLOGY V4.2 The Technology CPU is a standard SIMATIC CPU with integrated Motion Control functionality. This feature allows users to simply copy S7-300 programs from existing projects to new projects. The Technology CPU is programmed based on the SIMATIC programming languages LAD, FBD or STL. PLC and Motion Control functions are edited in a single application program. It is not required to learn any additional programming language. You can always fall back on your SIMATIC S7 knowledge. The Technology can be configured comfortably in STEP 7. There you can set all necessary parameters such as the mechanical data, drive selection data, controller settings, defaults, monitoring functions, output cams, measuring inputs, cam disks etc. ,,, SIMATIC S7-Technology is an options package used to configure Motion Control functionality of your Technology CPU. SIMATIC S7-Technology is fully integrated in STEP 7 after installation. Tools included in its installation: -Technology Objects Management -S7-Tech Library -S7T Config, including STARTER |
||||
Last edited by: dchartier at: 10/14/2012 5:23 PM |
|||||
This contribution was helpful to1 thankful Users |
11/7/2012 6:11 PM | |
Joined: 8/31/2005 Last visit: 5/21/2024 Posts: 2197 Rating: (326)
|
That is correct. |
|
|
Follow us on