4/26/2018 8:09 AM | |
Joined: 4/25/2014 Last visit: 11/1/2023 Posts: 7 Rating: (0) |
who can help me ?? |
4/26/2018 1:55 PM | |
Joined: 3/14/2008 Last visit: 8/10/2024 Posts: 2082 Rating: (931)
|
Make sure that during AS compilation the option: Set sampletime is checked (text maybe a bit different). All blocks with sampletime attribute is updated according to the OB they are in so the time is counted correctly. |
If I could help you, you can use the RATE button. Thank you. |
|
4/29/2018 6:10 PM | |
Joined: 4/25/2014 Last visit: 11/1/2023 Posts: 7 Rating: (0) |
I do not have these or similar options in "Settings for Compilation / Download"
AttachmentScreen_compile.pdf (70 Downloads) |
4/30/2018 9:02 AM | |
Joined: 3/14/2008 Last visit: 8/10/2024 Posts: 2082 Rating: (931)
|
Hi paahan, this is the wrong screen. The setting is located when you compile the AS, which is the button left of the download AS button in CFC editor.. |
If I could help you, you can use the RATE button. Thank you. |
|
5/9/2018 6:52 AM | |
Joined: 3/14/2008 Last visit: 8/10/2024 Posts: 2082 Rating: (931)
|
Hi paahan, Sorry for the delay... I saw your second screen, but can't see the option either, so I guess in your PCS7 version it's not yet available...Which version of PCS7+Cemat are you using? The only thing I can think of is that the hardware configuration of your CPU has been changed and downloaded after the reset of the CPU. You can assign each interrupt OB-> OB30-OB38 to a specific PIP range. You can choose whether OB32 is counted every second or 100 ms or..... Do you know if this happened or maybe you can cross check an old backup? |
If I could help you, you can use the RATE button. Thank you. |
|
5/13/2018 9:29 AM | |
Joined: 3/14/2008 Last visit: 8/10/2024 Posts: 2082 Rating: (931)
|
Hi, Quick answer: Only Cemat blocks must be installed only in OB1. Blocks from AP library for example (non cemat) must be installed in interrupt OB. |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on