5/13/2018 1:15 PM | |
Joined: 3/14/2008 Last visit: 8/10/2024 Posts: 2082 Rating: (931)
|
But you have given more info...can you tell me if the CPU cycling time exceeds 6000ms? Because then the CPU goes to protective state and all interrupt OB's times are reduced in half... A 500ms interrupt OB will take 1sec and if the cycling time still exceeds, the interrupt OB's are halved again.. You should get error messages in WinCC. |
If I could help you, you can use the RATE button. Thank you. |
|
5/15/2018 8:03 AM | |
Joined: 4/25/2014 Last visit: 11/1/2023 Posts: 7 Rating: (0) |
since the last CPU load 26 \ 04 \ 2018, the cycle time did not exceed 6000 ms |
Follow us on