5/19/2006 1:24 PM | |
Joined: 4/24/2006 Last visit: 7/12/2024 Posts: 8711 Rating: (1165) |
Hi Was, Perhaps the following link will help you: http://support.automation.siemens.com/WW/view/en/21950154 Shared variables are explained as follows: Shared User Data These are data or data areas that can be accessed from any point in a program. To use shared user-defined variables, you must create data blocks (DBs). When you create a DB, you define its structure in a structure declaration. Instead of a structure declaration, you can use a user-defined data type (UDT). The order in which you specify the structural components determines the sequence of the data in the DB. |
Last edited by: Wizard at: 5/19/2006 1:28 PMAnd of course the memory area of the CPU. |
|
Follow us on