6/20/2009 5:26 PM | |
Joined: 9/28/2005 Last visit: 8/27/2024 Posts: 2957 Rating: (242) |
Hi, Check this forum thread /tf/WW/en/Posts/5850 It should answer your question. |
Best regards, |
|
6/20/2009 10:01 PM | |
Joined: 10/3/2008 Last visit: 8/28/2024 Posts: 961 Rating: (124) |
Hi samker, this is possible. You can use "CPU Diagnostics". It's released for CPU 300 and 400. Wüstenräuber |
6/20/2009 11:51 PM | |
Joined: 7/2/2008 Last visit: 9/30/2024 Posts: 928 Rating: (308) |
Hello samkcr, I understand that you have 2 PCs. one with Simatic Manager installed and the other has WinCC. I'm afraid that all proposed solutions will require integration of WinCC in Simatic Manager to enable automatic message and tags transfer. I Recommend to finish all programming and leave this issue aside. When you finish, install WinCC on PC which has Simatic Manager and use report system error or any other proposed solution. I hope I understood your problem correctly. Best regards. H-H |
7/7/2009 11:07 AM | |
Joined: 9/7/2007 Last visit: 10/9/2024 Posts: 550 Rating: (62) |
Hi samkcr, You can find in this link several examples for the diagnostics of the CPU in the WnCC. There you can find all the needed sfc that should be added. |
Best Regards |
|
This contribution was helpful to1 thankful Users |
Follow us on