6/3/2015 7:34 AM | |
Joined: 12/22/2014 Last visit: 10/7/2021 Posts: 173 Rating:
|
Hello ilyanorsaelehe94 Can you post a screenshot of the message? Sometimes the Local Data (Priority Classes) has to be reconfigured. You can check the hardware properties of the CPU. In the tab Cyclic Interrupts you can see which priority is configured for your cyclic OB. In the tab Memory each priority is give a certain amount of Bytes. You can increase the amount if a cyclic OB needs more memory. If there really is no more spare memory, you can try to download the full program. |
Greetings |
|
6/4/2015 12:15 PM | |
Posts: 140 Rating:
|
Hello, You have to increase you load memory (EPROM), the datails of you memory can be seen in diagnostics of the CPU undet memry tab.. |
Follow us on