3/2/2015 2:28 AM | |
Posts: 2 Rating: (0) |
Hi Few months ago, the CPUs were fault and performed the diagnostic buffer. But it is difficult to know what is reason for the fault of CPU. The system is S412-5H, CPU redundancy(rack 0, rack 1), Power redundancy system (415Vac, 220Vac UPS, 110Vdc Battery). In accordance with site commissioning manager, the power have never disconnected before the detection of fault. The diagnostic buffer inform the event records as followings, It losses the main power, the back-up power supplied ( the terms between them is about 2 minutes). although of this, the memory was reset. Those it means the CPU 0 was fault? or the power supply unit for CPU is fault?
AttachmentCPU_Buffer.txt (343 Downloads) |
Last edited by: Min_Moderator at: 3/2/2015 10:35:32 AMMove buffer to attachment |
|
Follow us on