11/8/2011 4:37 PM | |
Joined: 4/24/2006 Last visit: 7/12/2024 Posts: 8711 Rating: (1165) |
Hello, Please have a look at the following link: how do you synchronize the date and time between an operator panel and an S7-300/S7-400 controller with WinCC flexible? Best regards, Wizard |
11/9/2011 9:10 AM | |
Joined: 4/24/2006 Last visit: 7/12/2024 Posts: 8711 Rating: (1165) |
Hello, It is possible to synchronize the CPU time by using NTP mode or SIMATIC mode. (It will be synchronized with another CPU or PC on the ethernetnetwork) how do you configure the SIMATIC S7-300 as time master or time slave for time-of-day synchronization via industrial Ethernet in SIMATIC mode? Which SIMATIC S7-300/S7-400 modules support the NTP time-of -day message and how do you activate this kind of time synchronization? how do you configure time synchronization? Time synchronization in the SIMATIC environment via MPI-Subnets BUT when you want to synchonize the time between CPU and HMI you should use the earlier mentioned method. Best regards, Wizard |
Follow us on