7/10/2020 4:45 PM | |
Joined: 3/14/2008 Last visit: 7/12/2024 Posts: 2076 Rating:
|
Hi, General information about updating the hardware catalog: You can update the hardware catalog by two options:
You can reach the update of the catalog by going to hardware configuration and selecting Options->Install HW Updates. You can then selection one of two options. If you don't have access to the internet, you can download the latest updates from the following link and install them manually by selecting the second option: Link The CPU410 in this case is only released for PCS7. For this reason, updates are provided via HUP's released for PCS7 which can be reached through the following link: Link At this point, a HUP for the 410 is only released for PCS7 V8.0 SP1. You will need to use the provided firmware V8.1 in your hardware configuration. |
Last edited by: Jen_Moderator at: 07/13/2020 08:28:08Optimized links. If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
2 thankful Users |
Follow us on