Industry Online Support
Technical Forum
11/5/2008 12:03 PM | |
Joined: 11/8/2005 Last visit: 6/5/2024 Posts: 335 Rating: (3) |
I want to use H-system with CP412-3H and CP443-1(6GK7443-1EX20-XXXX) in PCS7 V7.0 SP1.Is it possible or not? |
11/5/2008 12:14 PM | |
Joined: 10/3/2008 Last visit: 8/28/2024 Posts: 961 Rating: (124) |
Yes. Why should be this not okay? Wüstenräuber |
11/5/2008 1:39 PM | |
Joined: 10/3/2008 Last visit: 8/28/2024 Posts: 961 Rating: (124) |
Hi, which diagnostic messages are shown in diagnostic buffer? What happens? I found these: Info CPU: have a look at here: "The new CPUs can be programmed with STEP 7 V5.3 + SP2 and higher and Hardware Update HSP (Hardware Support Package)." Info CP: "The CP 443-1 EX20 can be projected as EX20 after STEP7 V5.4 SP3plus HSP. The installation instructions for a HSP you can download under 22374877. For the time being, operation with PCS7 is only permitted as spare part for the CP443-1EX11. A full release of the CP for PCS7 is in the planning stage." I know customers, who use the 1EX20 in PCS7 environment and it works. The functionality, which are used, is same like 1EX11. Wüstenräuber |
Last edited by: Wüstenräuber at: 11/5/2008 1:40 PM |
|
11/6/2008 7:46 AM | |
Joined: 11/8/2005 Last visit: 6/5/2024 Posts: 335 Rating: (3) |
Can I install hardware update HSP in PCS7 V7.0 SP1 for updating STEP7 V5.4 SP3? |
11/6/2008 9:02 AM | |
Posts: 433 Rating: (48) |
Yes, of course. Tomcat |
Follow us on