10/1/2013 10:01 AM | |
Joined: 12/12/2011 Last visit: 12/30/2020 Posts: 821 Rating: (41) |
Hello, do you have the project files? If yes, then you can define your own user/password an donwload it. If you don`t have the prject files, then you can try standard password user: admin pw: 100 in the online help you will find further information about user administration. regards, healthcheck |
Grundkurs/Systemkurs WinCC V7: |
|
10/1/2013 3:27 PM | |
Joined: 4/26/2012 Last visit: 10/13/2024 Posts: 1557 Rating: (169) |
link Look at the link, You'll have to create your users, and visible in the fields, or button, which calls the screen, filter by user group number. |
"Always make a backup before and check the best time before testing." |
|
10/3/2013 11:50 AM | |
Joined: 4/24/2006 Last visit: 10/14/2024 Posts: 8745 Rating: (1168)
|
Hello myhaye, It seems you have made some restictions to the button to change screen. (Only the Admin may change screen?) Or you use another user to login with lower permissions. (So the user and admin may change screen) And the input fields can be secured to be changed only by Admin. Tips and tricks for the topic of user administration Best regards, Wizard |
10/3/2013 7:19 PM | |
Joined: 4/26/2012 Last visit: 10/13/2024 Posts: 1557 Rating: (169) |
look at this too. good luck |
"Always make a backup before and check the best time before testing." |
|
10/4/2013 11:38 AM | |
Posts: 45 Rating: (0) |
hello, thanks for the cooperation, yes, only with admin user can navigate into the screens.in attach you can see what users and groups i have into my project, best regards, myhaye Attachmentprint screen.zip (259 Downloads) |
Last edited by: myhaye at: 10/4/2013 12:16 PManother think, i created another group "operator" and another user "op" with password. in users --->user "op" correspond to "user group" --->operator, save, rebuild, compile transfer to the panel (this is another panel for test MP277 10 inch), and when the application start on the panel, if i want to navigate between screens ask me about user and pass. I introduce user: op and pass: **** ---> ok after this navigate 2 ar 3 screens and again ask about password ---. cancel, again navigate 2, 3 screens ask me about password. best regards, |
|
Follow us on