2/26/2019 7:27 AM | |
Joined: 5/3/2017 Last visit: 5/21/2024 Posts: 673 Rating: (217) |
Hello Soroosh.v, in the manual PCS 7 APL Style Guide in section Creating project-specific blocks in conformance with APL you can find more information about how you can create your own block, blockicon and faceplates. With regards |
2/27/2019 10:01 AM | |
Joined: 8/19/2017 Last visit: 7/9/2024 Posts: 79 Rating: (3) |
Hi Heisenberg2 This is a very good manual for creating blocks from basic. The problem is that I don't want to create a block from basic, I just want to use a CEMAT block with all of it's capabilities inside a user block. The user block doesn't need any faceplate itself, it should use the main block I/Os and faceplate and only some of the parameters changes inside the user block, the other I/Os and faceplate are the same. I attached an example of what i'm going to do (this is not a complete example). Thank you. |
Follow us on