5/11/2017 7:22 AM | |
Joined: 3/14/2008 Last visit: 7/12/2024 Posts: 2076 Rating:
|
Hi Microman, You always have interesting questions For a Danfoss drive, we use the following code:
We use "GADR_LGC" (SFC5 from the standard library->System Function Blocks). You can get the base address of the input/output module of the slave by setting the profibus address->variable "LADDR". We use it with profinet as well. It is not really a DRIVER block, because a driver block is the interface between your CFC program and hardware modules...In order to create a driver block, you will need to write a GSD file I believe so the system can create the interconnection. See the attachment for a print screen of the special function. |
Last edited by: Oreca at: 5/11/2017 7:24:05 AMIf I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
2 thankful Users |
Follow us on