5/1/2017 3:05 PM | |
Posts: 24 Rating:
|
I have my own FB, which is a motor block and I coded it by SCL. I've read BST exm , and the PCS7 APL styleguide. I've actually read the below pdf and some others Attachment1_PCS7_APL_Styleguide_en_EN_en-US.pdf (755 Downloads) |
5/3/2017 10:13 AM | |
Joined: 10/26/2011 Last visit: 6/12/2024 Posts: 762 Rating:
|
You have found the right document. But Siemens recommends to use standard. Standard means to use the Advances Process Library Library (APL) and Industry Library (IL). Additional you can work with the Siemens add-on libraries like CEMAT, SITRANS library, etc. If you create your own blocks and faceplate, it could be possible, that you get in trouble by updating newer versions. --- You cannot use the motor blocks from the APL Library? |
Last edited by: Thunderstorm at: 5/3/2017 10:25:31 AMSIMATIC PCS 7 - Overview |
|
5/3/2017 12:27 PM | |
Joined: 3/14/2008 Last visit: 7/12/2024 Posts: 2076 Rating:
|
Hi, I responded to several topics about creating your own SCL blocks in compliance with APL. See below for a few topics which should help you. |
If I could help you, you can use the RATE button. Thank you. |
|
5/7/2017 6:50 AM | |
Posts: 24 Rating:
|
thanks, before posting my question, I really used alot of your previous answers to posts, I have read all of them, the sequence is similar which you explained, but I need more help, for example for creating my own block icon which I can make my motor block icon to operate in on ,off, error mode, with different appearance and colors, and connecting it to my own SCL block and its faceplate. Attachment16514590_pcs7_create_own_block_icons_v8x_en.pdf (501 Downloads) |
Follow us on