1/22/2015 11:38 AM | |
Joined: 3/14/2008 Last visit: 7/17/2024 Posts: 2078 Rating: (931) |
Hello @L4N, 1. You can create user defined batch reports by creating .rpt files in the folder: C:\Programs\SIEMENS\BATCH\Template. The recommended procedure is to copy the batch report templates of the "standard" template library to this folderand change the name. 2. Open Batch CC 3. Open the project settingsof your project ->Tools->Settings->Project Settings 4. In project settings, select Report and select the required batch template. Make sure you create a copy of the standard template. If you do not do this, it is possible that you havea template that does not include a combination ofobject type and family. Then the report is created in SQL database, but when printed or displayed it shows no content. Also make sure that during a new installation, the template directory is overwritten, so you have to copy your own template back to the folder. Is this what you want? Best regards |
If I could help you, you can use the RATE button. Thank you. |
|
1/22/2015 11:43 AM | |
Joined: 3/14/2008 Last visit: 7/17/2024 Posts: 2078 Rating: (931) |
I got some info for you on how to adjust a standard template from the siemens site. Grtzz!! Configuration Notes: Description:
Example:
|
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
Follow us on