2/6/2015 9:05 AM | |
Joined: 5/12/2006 Last visit: 7/11/2024 Posts: 22308 Rating:
|
Hello, no this is not possible. SIMOTION doesn't support USS. Regards Christoph |
2/6/2015 9:38 AM | |
Posts: 153 Rating:
|
Thank you for the prompt response. I suspected that but thanks for the definitive answer. |
2/6/2015 12:38 PM | |
Joined: 9/24/2008 Last visit: 6/19/2024 Posts: 30 Rating:
|
I'm not sure that this is strictly true? It is possible to use the CP340 and CP341 with Simotion, if using with Simotion D connection would have to be via IM153. There is a function manual that covers the supported functions. https://support.industry.siemens.com/cs/attachments/98967702/CP_Functions_en-US.pdf?download=true Nick |
Last edited by: HMK_Nick at: 2/6/2015 12:49:56 PM |
|
Follow us on