10/26/2007 9:54 AM | |
Joined: 10/19/2005 Last visit: 11/30/2020 Posts: 1611 Rating:
|
Hi, did you have looked into the manual from the MP277? There are a good description about the message 70011 and what you can do! -> http://support.automation.siemens.com/WW/view/en/23337820 regards, |
8/31/2023 2:28 PM | |
Joined: 6/18/2020 Last visit: 2/12/2024 Posts: 11 Rating:
|
Dear Brain, The same error and same issue i m facing in TP900 HMI. The link you mentioned is not opening, and showing page error. Tried on different brower as well. Kindly assist me with this and update the link. |
9/12/2023 9:37 AM | |
Joined: 8/3/2009 Last visit: 7/31/2024 Posts: 13425 Rating:
|
Hello Check if you use the correct timestamp in your PLC datatype: https://support.industry.siemens.com/cs/ww/en/view/109813307/89327861387 You also have to check if the Weekday fits to your date!!! if this is not set or logically wrong then also an Error will occur Use Date_and_Time or DTL Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on