4/28/2017 9:34 AM | |
Joined: 7/30/2012 Last visit: 8/1/2024 Posts: 335 Rating: (12) |
Hi... I'm Having trouble In Creating DCC Chart I'm Getting Error Message About Publishing I Have Attached Program Backup Can Anyone Help Me To Come Out From This ??? AttachmentDcc_Chart_Test.zip (399 Downloads) |
4/28/2017 11:04 AM | |
Joined: 4/18/2011 Last visit: 8/6/2024 Posts: 2 Rating: (1) |
Dear KB The Beginner, to connect SINAMICS parameters with DCC-Blocks it is mandatory to publish the respecting "docking"-parameters in DCC. Therefor you need to apply to the defined semantic: Creating a BiCo: @*<number> <NAME> Between <number> and <NAME> a blank space is needed. The triangle brackets <> must not be typed in... Such BiCos will be seen in the expert list (=published) an can now be treated like common expert list parameters. Please note that the date type must be identically in case you want to connect them with a parameter. You missed to publish the input parameter in DCC which you connected to r482. And you missed to insert the "*" while publishing the output parameter you connected to p2530. Additionally you published parameter 0 as a "setting parameter" (such parameters appear in green when leaving the "*" between @ and the parameternumber). Such "setting parameters" can never be an output of a DCC-Block. Usually this "intermediate" signal is not needed to be published. You find all this fundamentals in the DCC manual: https://support.industry.siemens.com/cs/ww/en/view/27032481 Please refer to page 52 for detailed explanations and figure out attachment. Good luck! AttachmentTest_320_runningDCC.zip (411 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on