10/6/2020 12:53 PM | |
Joined: 3/14/2008 Last visit: 7/12/2024 Posts: 2076 Rating: (930)
|
Hi, Do you mean deleting a selected multiproject? You can do so via Simatic Manager via File->Delete and select column: Multiprojects to delete the multiproject or column Projects to delete individual projects |
If I could help you, you can use the RATE button. Thank you. |
|
10/6/2020 2:57 PM | |
Joined: 2/1/2010 Last visit: 7/12/2024 Posts: 148 Rating: (71) |
If you mean to make it so Step7 does not display the other projects from those available in the list when using the File>Open command without deleting? You can use the File>Manage command to hide or display projects from the list. If you mean to just clear the MRU (most recent used) list inside SIMATIC Manager, you have to edit the Windows registry in order to clean up the list without deleting projects (or opening other things like libraries to push the project you don't want to see anymore off the MRU list). - I don't recommend this and hold no liability if you corrupt your installation by following this hint. "s7tgtopx\Recent Object List" |
If my post helped you, please rate. Thanks. |
|
Follow us on