5/12/2020 2:03 PM | |
Joined: 11/8/2017 Last visit: 5/27/2024 Posts: 322 Rating: (175) |
Hi, In the Evaluation Editor, you can use the Script function for the Expression. An example I've used before is to use the 'Math.max' function at the start of the script. Use this to read the maximum value of multiple binary points. If any of the binary points goes to a 1 (i.e. On), then the condition is applied. I've attached an example, hopefully it makes sense. Adapt the contents of the text file as required, and paste into the Expression box in the Evaluation Editor. Although this shows the solution being applied to the 'Visible' property of an item, a similar principle can be applied on other items to achieve what you're looking for (i.e. the Blinking property). Regards,
AttachmentExample.zip (281 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on