7/7/2023 9:06 AM | |
Joined: 6/4/2010 Last visit: 8/13/2024 Posts: 387 Rating:
|
Dear forum member, This Desigo CC remote notification functionality involves using the Event Cause and/or "Customer Text” fields present in the Trigger Rules when configuring Notification Incidents. Event List SOURCE Field = Notification CUSTOMER TEXT Filter trigger As far as I know, the "Customer Text" is configured in the device connected to Desigo CC. For example, when configuring Sinteso FS20 fire panels or Algorex CC11 fire panels, it is necessary to import the panel configuration files. This configuration file includes a panel ID, the panel description (the client text, if configured), and the number of instances, or objects, that belong to each panel. (See image 3) Screenshot 2 – 3 – 4 – 5 are an example of an event (Exclusion) of a zone with "CUSTOMER TEXT" configured (see image 4) and an example of an event (Exclusion) of a zone without "CUSTOMER TEXT" configured (see image 5) Event List CAUSE Field = Notification EVENT CAUSE Filter trigger If, on the other hand, in the trigger you want to use the "Event Cause" field then you have to pay attention to the "Text Group" associated with the "Present Value" of the object you want to check and then fill in the trigger with one of the tests available in the "Text Group" Screenshot 6 – 7 – 8 - 9 Best regards, Albis AttachmentScreenshotsReNo.docx (386 Downloads) |
Follow us on