Industry Online Support
Technical Forum
1/2/2024 7:07 AM | |
Joined: 12/15/2016 Last visit: 6/28/2024 Posts: 56 Rating:
|
Hello, I am having an error intermittently on an IOT and I do not understand the cause of the problem. After several days that the IOT2050 is running its port 'eno1' stops working. If I enter the IOT2050 via another port and ping some network device that is connected to 'eno1', it tells me 'Destination host unreachable'. (Image attached) From another device connected to the network where the 'P1' of the IOT is, I try to ping the 2 IP's that the IOT2050 has and it is not accessible. (Image attached) The configuration is normal, in the 'eno1' it has 2 IP's configured, something standard, I have even disabled IPv6 (Attach image) Port 'P1' status LED is active. All I can do is restart the IOT to get the port to work, then after a day (random) it crashes again. It's not urgent, but could you help me with this issue, please. Thanks, Attachmentdata.zip (216 Downloads) |
2/22/2024 10:16 AM | |
Joined: 12/15/2016 Last visit: 6/28/2024 Posts: 56 Rating:
|
Hello, I'm still having this problem and on different IOT2050 Basics with different configurations. I attach images of a 2nd IOT with the same problem. I fix the problem by rebooting. Is this happening to anyone else? In case there is no solution, is there any 'code+task' to be able to fix the problem without restarting? Thanks, Edu
Attachment1.zip (187 Downloads) |
Follow us on