9/17/2015 10:04 PM | |
Joined: 2/8/2015 Last visit: 7/10/2024 Posts: 462 Rating: (9) |
Hi Christoph D, The version of TIA is V13 SP0 UP0. This project works good when the connection interface between HMI & PLC is PROFINET. I have the problem every time i have changed the connection interface from PROFINET to PROFIBUS. The attached file shows this. I have another questions from Device proxy : 1) Why FB, FC & OB can't come to TIA project, but DB can to be in TIA project ? 2) Is the function " Device proxy " supported by TIA Portal V12 ? Best regards Tekabi AttachmentDevice_Proxy_Prob.zip (266 Downloads) |
Last edited by: Tekabi at: 9/17/2015 10:14:27 PM |
|
9/18/2015 6:23 PM | |
Joined: 5/12/2006 Last visit: 9/3/2024 Posts: 22352 Rating: (3008) |
Hello, the latest Update for V13 without SP1 you find here: https://support.industry.siemens.com/cs/ww/en/view/90466591 Regards Christoph |
9/20/2015 12:40 PM | |
Joined: 2/8/2015 Last visit: 7/10/2024 Posts: 462 Rating: (9) |
. |
9/20/2015 2:19 PM | |
Joined: 12/18/2014 Last visit: 9/13/2024 Posts: 33758 Rating: (4191) |
Are you bored? |
Follow us on