6/6/2017 12:54 PM | |
Joined: 12/9/2010 Last visit: 10/8/2022 Posts: 623 Rating: (76) |
Hi MashV, For reading 4 bytes of diagnostics data, u should use SFC51 with SSL-ID :W#16#00B1. INDEX-- Bit 0 to bit 14: logical base address Bit 15: 0 = input, 1 = output |
If you like the comment, rate it (right top) or thank it (left bottom). |
|
This contribution was helpful to1 thankful Users |
6/7/2017 6:28 PM | |
Joined: 12/9/2010 Last visit: 10/8/2022 Posts: 623 Rating: (76) |
Hi MashV, U can download the manual of the CP341 and u will find same thing. Byte 1-Bit 0 to bit 3: Module class (CPU, FM, CP, IM, SM, ...). So it includes CP diagnostics info. |
If you like the comment, rate it (right top) or thank it (left bottom). |
|
Follow us on