8/14/2023 9:45 AM | |
Joined: 12/6/2022 Last visit: 8/17/2023 Posts: 1 Rating: (0) |
I am on Windows 11. The installation of Digsi 4.93 stops at Prerequisites with following message: "Siemens DIGSI V4.93 Setup Wizard ended prematurely because of an error". The setup log file is as follows: [snip] I have already clean installed windows 11 but still not working. Please help. AttachmentSetup_Log.txt (572 Downloads) |
Last edited by: Jen_Moderator at: 08/15/2023 05:43:57Setup log added as .txt file. |
|
4/9/2024 3:38 AM | |
Joined: 10/6/2017 Last visit: 8/21/2024 Posts: 2 Rating: (0) |
Hi i facing a problem when i reinstall back my Digsi 4.95 on the same PC.(Win10) The error is "Siemens DIGSI 4.95 Setup Wirzard ended prematurely because of an error" Btw, i have uninstall the same version twice and retry..but unfortunately it keep failed during setup/ The reason i deleted the existing one is because the trial ended. and i planned to reinstall it using serial number AttachmentSetup_Log.txt (411 Downloads) |
Follow us on