7/1/2022 11:05 AM | |
Joined: 7/1/2022 Last visit: 10/3/2023 Posts: 2 Rating: (0) |
Installed: SIMATIC WinCC flexible Runtime 2008 SP5 OS: Windows 10 LTSC 1809 (OS Build 17763.2565) (64-bit) Everytime a restart Windows I lose LogDevices files for my TCPIP ethernet card. Gone: If I manually Restart service “S7DOS Help Service” I can get my files back: And then i can config Set PG/PC Interface These are the Siemens Services that are always Running after reboot: I have tried to repair SIMATIC WinCC flexible Runtime 2008 SP5 in Add/Remove programs but that didn’t help. Has anyone had similar problem? Any tips that I can use to troubleshoot this issue? It seems the service is not working or cannot do its job at Windows startup. Is it supposed to refresh LogDevices after each reboot? BR Lars-Olov Sandström AttachmentWinCC problem.zip (591 Downloads) |
Last edited by: larsanswe at: 07/01/2022 13:33:27 |
|
7/5/2022 3:27 PM | |
Joined: 8/3/2009 Last visit: 9/6/2024 Posts: 13594 Rating: (1720)
|
Hello do you have tried to use the latest Update for WinCC flexible 2008 SP5?: https://support.industry.siemens.com/cs/ww/en/view/109757233 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on