1/25/2007 8:35 AM | |
Posts: 3149 Rating: (171)
|
Hi which version of WinCC flexible 2005 are you using? Did you already install SP1 + HF6? http://support.automation.siemens.com/WW/view/en/23059737 http://support.automation.siemens.com/WW/view/en/24376196 nemo |
1/25/2007 2:31 PM | |
Joined: 10/6/2005 Last visit: 2/26/2024 Posts: 44 Rating: (0) |
I only have SP1. I will download HF6 and see if that helps. |
7/21/2007 10:33 AM | |
Posts: 3 Rating: (0) |
Hi Charlesm, Can u post the script that you are using for displating current screen name. |
6/22/2011 2:43 PM | |
Posts: 11 Rating: (0) |
Dear Charlesm, I had the same problem when i have deleted the "TemplateTextFieldScreenname".So just add it in the "Template" and see the result. Regard. |
5/22/2014 4:38 PM | |
Posts: 9 Rating: (0) |
Hi, Can you please walk me through the steps to create such deleted template??? Thank you in advance.
|
5/22/2014 4:46 PM | |
Joined: 11/26/2011 Last visit: 6/29/2023 Posts: 508 Rating: (23) |
"TemplateTextFieldScreenName" - It contains the screen name on every screen. Check for this object on the screen. |
5/22/2014 4:55 PM | |
Joined: 1/21/2013 Last visit: 10/8/2024 Posts: 4620 Rating: (708) |
Hello Mauricio Giraldo, Have you already seen this: Help me ...About layer 0 is error...when runtime... |
Follow us on