10/29/2019 1:50 PM | |
Joined: 5/28/2015 Last visit: 1/5/2022 Posts: 3 Rating:
|
Hello, I have the same problem. I bought a TM31 module 6SL3055-0AA00-3AA0 and would like to connect it to a CU320-2PN controller. Fault: Immediately: 04.01.00 20:47:00:438 Drive_unit_1 : Input_output_component_1 -- 1360 : Topology: Actual topology not permissible(Fault cause: 8, preliminary component number: 203) Fault: Immediately: 04.01.00 20:47:00:422 Drive_unit_1 : A_INF_03 -- 1360 : Topology: Actual topology not permissible(Fault cause: 8, preliminary component number: 203) Fault: Immediately: 04.01.00 20:47:00:374 Drive_unit_1 : SERVO_02 -- 1360 : Topology: Actual topology not permissible(Fault cause: 8, preliminary component number: 203) Fault: Immediately: 04.01.70 20:46:51:262 Drive_unit_1 : CU_S -- 1360 : Topology: Actual topology not permissible(Fault cause: 8, preliminary component number: 203) Does that mean that I have no chance to make the TM31 module 6SL3055-0AA00-3AA0 work with my CU320-2PN and I have to buy a TM31 6SL3055-0AA00-3AA1 module?
------------------------------------------------------------------------------------------ |
Last edited by: ReiRau at: 10/29/2019 16:50:19Last edited by: Jen_Moderator at: 10/30/2019 09:35:02New subject after splitting |
|
10/31/2019 9:42 AM | |
Joined: 5/28/2015 Last visit: 1/5/2022 Posts: 3 Rating:
|
Thank you for the clarification. Best regards Reiko |
Last edited by: ReiRau at: 10/31/2019 09:42:42 |
|
Follow us on