5/20/2015 12:29 AM | |
Joined: 9/3/2014 Last visit: 3/7/2024 Posts: 79 Rating: (4) |
Hi Mr ChristophD I am grateful for your quickly answer, it has been very helpful, I only need Vector Control Mode, but I don't understand something, may be you can help me, my motors are AC voltage and all of them have one Resolver 5.5 Volts and 10 KHz, (for each one), I was trying to put a Control Unit CU 250 DP because it lets me connect a Resolver sensor but when I was setting the parameters I can´t find Resolver like an option, only Encoder, I don´t know, How can I connect "physical connection" my Resolvers to my control units, Do I have to buy a SMC10 module for each one?, What is terminal interface, SUB D interface, Drive - Cliq interface?, I know that I can connect a Resolver with S120 through Drive - Cliq interface but no for G120 coverters. Excuse me if my doubts are basics, but I am new in this thematic and I need help from experts. I will be grateful if you can help me, Thanks in advanced. AttachmentImages.pdf (234 Downloads) |
5/20/2015 3:15 PM | |
Joined: 9/3/2014 Last visit: 3/7/2024 Posts: 79 Rating: (4) |
Hello Dear Expert, I am grateful with your help, I am learning with your tips, I attach you a PDF file with some photos about the actual converter and the resolver's connexion , it has DB9 connector, I haven´t could find Resolver option How can I connect the Resolver to my Control Unit CU250, Do I need to buy anything else? I will be grateful if you dear expert can help me. I'm still confused in some things. AttachmentImages.pdf (172 Downloads) |
Follow us on