9/13/2013 8:33 AM | |
Joined: 4/22/2010 Last visit: 5/3/2024 Posts: 5697 Rating:
|
Hello, Let's start with the manual: SIMATIC HMI HMI device OP 73, OP 77A, OP 77B (WinCC flexible) And then What transfer options are available in the various operator panels? There you also find a list with cables to use. You cannot transfer he project with step7. Step 7 opens Wincc flexible (if option intergrate in Step 7 is selected in Wincc) and then you can transfer with Wincc Flex. Regards, Marcjan |
Problem solved? |
|
9/13/2013 11:45 AM | |
Joined: 1/21/2013 Last visit: 6/6/2024 Posts: 4620 Rating:
|
Hi What does it mean not compatible? with WinCC Flex 2008 SP3 can open all programs with previous versions, but not vice versa. Have a look: If i have wincc flexible 2007 is possible to open a project that had created in older or newer version of my software? |
9/13/2013 1:25 PM | |
Posts: 34 Rating:
|
In a shorter way, will the firmware of the actual OP73 be udpated to 1.7 by the transfer via WinCC Flexible? |
Follow us on