Industry Online Support
Technical Forum
9/13/2013 2:10 PM | |
Joined: 4/24/2006 Last visit: 7/12/2024 Posts: 8711 Rating:
|
Hello Romam, When you try to transfer project to OP73, you will get a warning. (Telling you that the panel needs an OS update) WinCC flexible will try to do it. Otherwise you will have to do it yourself. how do you do an operating system update (OS update) on operator panels? After that you can transfer your project to panel. Best regards, Wizard |
9/16/2013 7:35 AM | |
Posts: 34 Rating:
|
I can add that the CP of the PG is CP5711 |
9/16/2013 9:19 AM | |
Joined: 4/24/2006 Last visit: 7/12/2024 Posts: 8711 Rating:
|
Hello Romam, Perhaps this link might help: how can you transfer a WinCC flexible project via MPI/PROFIBUS to a Windows-based panel? Best regards, Wizard |
9/16/2013 3:17 PM | |
Posts: 34 Rating:
|
OP73 doesn't look "windows based". And unlike in your tutorial, MPI/DP is exactly the same on the OP73. You can't separate them. Enable/disable, rem on/off , adress and baud rates are the only parameters you can modify. |
9/17/2013 11:22 AM | |
Posts: 3037 Rating:
|
Hello, You can use this FAQ for OP73 too. how can you transfer a WinCC flexible project via MPI/PROFIBUS to a Windows-based panel? Tweety |
Follow us on