6/27/2023 5:33 AM | |
Joined: 3/14/2008 Last visit: 8/10/2024 Posts: 2082 Rating: (931)
|
Hi, Siemens has been integrating consistency to PCS7. For example, if a compile was cancelled, a full compile is needed. Also when creating backups, secure archiving will check the program for inconsistencies. However, I suggest you back up this project and hope you have created a backup before you did the changes. Check if you can download the older backup with changes. Maybe the error came soon enough and the controller is "untouched". If you do not have a recent backup, then the only way is to download in full. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to2 thankful Users |
6/28/2023 7:26 AM | |
Joined: 2/6/2015 Last visit: 7/28/2024 Posts: 19 Rating: (0) |
Base on the picture, do you know why there was an error during download? What is the error mean? |
6/28/2023 7:34 AM | |
Joined: 3/14/2008 Last visit: 8/10/2024 Posts: 2082 Rating: (931)
|
Hi, It could be several things like CPU defective, CP card defective, Ethernet cable connector or cable problem, human intervention (someone bumped the communication cable or removed the wrong one), problem in the Ethernet card in the ES, problem in the ES, problem in the project itself (blocks folder/CFC charts). You can check the diagnosis of the CPU, maybe the root cause is found there. |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on