3/24/2007 9:14 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (318)
|
Dear Kolma, Which Lean card do you have and which STEP7 version, the CPU-type and firmware version could be also a problem. Normally it must be possible to program over Ethernet (LAN) to the CP343-1 Lean. It might also a problem when the CPU you are using is some older. See also the list with compatible CPUs and CPs as of V5.0 SP3 HF3 Routing-compatible SIMATIC S7 modules as from STEP 7 V5.0 SP3 HF3 What requirements must be fulfilled and what should I watch out for when executing Routing? |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on