2/4/2016 9:16 AM | |
Joined: 3/30/2009 Last visit: 3/12/2024 Posts: 10 Rating: (2) |
The download file ends with error. Someone else to this problem? Thank's a lot Best regard |
2/4/2016 11:16 AM | |
Posts: 1 Rating: (0) |
Yes, me too, the file is not complete. Someone can help? |
2/11/2016 8:41 AM | |
Posts: 1 Rating: (0) |
startdrive_optional_v13_sp1.zip is the name of the file theat end with an error.(you can see the error in attachment, with italian Language). Liliano |
10/29/2019 10:37 AM | |
Joined: 3/9/2018 Last visit: 12/28/2023 Posts: 57 Rating: (0) |
dear sirs the program is not loaded. any help please? |
11/20/2020 10:18 AM | |
Joined: 3/26/2020 Last visit: 11/2/2023 Posts: 1 Rating: (0) |
Hi everyone, I need to download SINAMICS Startdrive V13 SP1. thanks. |
Follow us on