7/9/2013 9:58 AM | |
Posts: 515 Rating: (56) |
hi, you have the HMI software with you?(wincc flexible) or only the program backup?
|
7/9/2013 10:13 AM | |
Joined: 3/18/2008 Last visit: 12/8/2023 Posts: 1750 Rating: (272) |
Hello, you need to download .HMI file to MP277. For that you need WinCC Flexible Software & Communication cable(ethernet/MPI Adaptor). Also, Have a look at following FAQ's. How can you transfer a WinCC flexible project via Ethernet to a Windows-based panel? How can you transfer a WinCC flexible project via MPI/PROFIBUS to a Windows-based panel? |
Last edited by: Amit_86 at: 7/9/2013 10:27 AMVANDE MATARAM..... |
|
7/9/2013 12:15 PM | |
Joined: 4/19/2008 Last visit: 9/3/2024 Posts: 1525 Rating: (159) |
Hello Jimshad, You can used the Pack & Go Function, if you dont Have Software with you.. Have A look on FAQ. How can you transfer a WinCC flexible configuration without configuration software to an operator panel (Pack&Go)? With WinCC Engineering (TIA Portal), how can you transfer an HMI configuration without configuration software to an operator panel (Pack&Go)? |
Ammy |
|
7/12/2013 7:07 AM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181) |
It is possible that both files will not do a job. And also will not possible to take a new backup because of
A useful link for future usehttp://support.automation.siemens.com/WW/view/en/27873792 |
This contribution was helpful to1 thankful Users |
Follow us on