7/28/2022 8:45 AM | |
Joined: 7/14/2017 Last visit: 9/2/2024 Posts: 7 Rating: (0) |
HI, I am having a pack & go backup given by OEM that was created in TIA WINCC V14sp1 with image version v12.0.0. So when I try download it using pack&go the message comes is "Transfer Failed" in pack n go window. So, i Simulated the conditions using TIA v14 sp1. created a dummy pack n go backup for TP700Comfort for Image versions. v12.0.0, v13.0.0, v14.0.0. After trying found similar issue with v12.0.0 image. whereas, it asked for downgrading the image in V13.0.0 & V14.0.0 pack n go( Communication established ). So, i thought there might be some problem in v14 sp1. so i installed TIA Wincc V12 & Simulated the conditions using TIA v12 sp1. created a dummy pack n go backup for TP700Comfort for Image versions. v12.0.0. but problem remained same. Can any one Help in this regard??? Mode:- Ethernet IP- 192.168.0.2 HMI- TP 700 Comfort (Image version V15.0.0) {Out of Box} ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/28/2022 11:52:14New subject after splitting |
|
7/29/2022 8:20 AM | |
Joined: 7/14/2017 Last visit: 9/2/2024 Posts: 7 Rating: (0) |
Hi Murof, Yes simatic prosave has been installed on the PG. |
9/1/2022 7:19 AM | |
Joined: 7/14/2017 Last visit: 9/2/2024 Posts: 7 Rating: (0) |
THANKS :-) |
Follow us on