4/6/2016 7:09 AM | |
Joined: 3/14/2008 Last visit: 6/4/2024 Posts: 2070 Rating: (928) |
Goodmorning! Those driver blocks are from the old PCS7 library: PCS7 7.1 SP3, so called "Classic" library. This library is included in the PCS7 DVD of your version (I believe Disk2). Are you using an old version which you want to migrate? Or are you starting a completely new project? In case your start new, I highly suggest you start with using the APL library, because that is the Siemens standard since PCS7 7.1. The Classic library is only for migration projects, without the use of new functionality. The libraries are very different from one another, but APL delivers much more for the user and looking at the future (continues expansion, support etc), APL is the way to go! See the following link for the APL library: APL Library Please let me know if you have any more questions.... |
Last edited by: Oreca at: 4/6/2016 7:14:52 AMLast edited by: Oreca at: 4/6/2016 7:16:45 AMIf I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
4/6/2016 7:52 PM | |
Posts: 39 Rating: (2) |
Thank Oreca and mark1507. You really helped me. Yes, I create a new project. I will study the APL library |
Last edited by: jkrinicky at: 4/6/2016 7:57:02 PM |
|
4/7/2016 7:30 AM | |
Joined: 3/14/2008 Last visit: 6/4/2024 Posts: 2070 Rating: (928) |
OK, Good! Have fun! Maybe it's good to take a look at the following link: Its the complete overview of PCS7. I suggest you will use the following two manuals: Getting Started Part 1 (v8.1 with APL) and Getting Started Part 2 (v8.1 with APL) These are basic knowledge about PCS7. You can use the following manual to get you started with an example project, where APL blocks are used See Link These manuals will get you started and you can use the APL library (link in my previous post) as a reference. |
Last edited by: Oreca at: 4/7/2016 7:33:23 AMIf I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
4/7/2016 6:41 PM | |
Posts: 39 Rating: (2) |
Oreca, Thank you very much for these manuals. Undoubtedly, these books help me learn PCS7 |
Follow us on