8/14/2019 4:16 PM | |
Joined: 11/15/2018 Last visit: 7/13/2023 Posts: 10 Rating: (0) |
Hi, I am having some communication issues when trying to backup/download from Siemens PG to an OP Panel using Protool(V6.0 SP3) and Prosave(V9.0.3.0). I have read through a lot of online forums on similar issues but can't figure out why I am having issues I have an OP17 panel(6AV3617-1JC20-0AX1) which needs to be replaced so I plan to take a backup of the program from the panel and download it to another OP17 panel (Exact same part number, new in box). I have tried to take a backup using Prosave as described here but I get a commuication error "Could not establish a connection. Check your settings, interfaces, cables, etc". In the 'General' tab in Prosave I have the following settings: Device Type: OP17 Connection: Serial Port: COM1 Baude Rate: 9600 I have tried the other Baud rate settings and the other COM2 port option but none seem to work. The cable I am using is 6AV3617-1JC20-0AX1 and the OP is in transfer mode so everything looks fine. I have also tried to create a basic project in Protool and try to download to the OP but get error message "E4027: Synchronization faulty. No connection to the OP!" in the download window. The settings i have in File>Download>Preferences are similar to Prosave settings described above and have tried various other settings. If anyone could offer any advice for a solution for this would be great. |
Follow us on