4/6/2024 2:33 AM | |
Joined: 12/18/2014 Last visit: 9/15/2025 Posts: 35961 Rating:
|
What kind of encoder is this? What speed are we talking about? |
4/7/2024 11:17 AM | |
Joined: 1/9/2022 Last visit: 8/21/2025 Posts: 34 Rating:
|
encoder resolution is 100 PR |
4/7/2024 1:18 PM | |
Joined: 6/11/2019 Last visit: 9/14/2025 Posts: 2630 Rating:
|
- At 1155 rpm that would be 19.25 ups. - 19.25 and an incremental sensor of 1:100 that would be 1925 pulses per second. - 1925 pulses * 2 seconds sampling frequency = 3850 pulses per 2 seconds. This is possible with the logo.Therefore just set the value P4 from B002 to 100 (see example). Ella_68 AttachmentProgrammplan-3.zip (627 Downloads) |
5/3/2024 4:09 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8171 Rating:
|
New question published by Thien Tam is split to a separate thread with the subject Which input pin can be used to read the high speed pulse signal sent by the encoder?. Best regards |
Follow us on