6/10/2015 5:19 PM | |
Joined: 9/22/2008 Last visit: 6/11/2022 Posts: 30 Rating: (3) |
dear all, I need help! We have WinCC project that is stand alone (no clients) just one PC. We want to have engineering station on which we can edit (maintenance) our WinCC project and then download to OS, or to sichronize projects. I know how to do that with multi-user (server-client )projects. But I don't know what is solution when project is stand alone?
Thanks!!
---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 6/11/2015 1:20:36 PMNew subject after splitting |
|
6/11/2015 4:29 AM | |
Posts: 43 Rating: (7) |
Hello makijato, The procedure is similar as you do it for multi-user project In ES, project wizard select "single station" while creating the project
|
6/15/2015 7:24 AM | |
Joined: 10/3/2010 Last visit: 5/29/2024 Posts: 1552 Rating: (188) |
You can find examples in the PCS7 Engineering System - Configuration Manual First make sure that Simatic Shell is fine and that the folder above the one containing your WinCC-project is shared for the right users. Open Simatic Manager on your ES computer, create a new ES-project. Select the mcp-file and click Open (Make sure project is not open, not running). Click on Import OS. After succesfull import, you'll see your WinCC-project in your ES as SIMATIC PC Station(1) as WinCC Appl. Rightclick on SIMATIC PC Station(1)and choose Object Properties and rename. Afterwards, rightclick on the name of your WinCC-project and choose Object Properties, go to tab Target OS and Standby OS, check or change Path to the Target OS Computer. |
B r g d s , |
|
This contribution was helpful to1 thankful Users |
6/16/2015 5:21 PM | |
Joined: 9/22/2008 Last visit: 6/11/2022 Posts: 30 Rating: (3) |
Thank you, SteBo! I will try these days :) |
Follow us on