5/2/2022 8:40 AM | |
Joined: 4/28/2015 Last visit: 10/22/2024 Posts: 1278 Rating: (300) |
Hi, the FB283 was made for that purpose: https://support.industry.siemens.com/cs/de/en/view/25166781 The application text doesn't name V90 (as it was not available back in that time) but it should work same way. One important parameter is the "AXIS_NO" (axis number) - the document explains which one to use for which drive but doesn't show V90 of course. As far as I can remember here you need to use the value "2" for V90 - if this does not work then it must be "1". |
Best regards, |
|
5/9/2022 7:25 AM | |
Joined: 3/13/2014 Last visit: 9/12/2024 Posts: 56 Rating: (1) |
Hi RB91, Thanks for your reply, have you used FB283 for v90 communication in simatic manager..? I don't received v90 hardware yet for testing the block logic, so i am afraid wether this block will work or not for v90 drive communication.
|
Follow us on